AKD Setup Wizard...
- The scan has been performed
- Your project is compliant with the physical devices on the EtherCAT
***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs network - You have activated the Online Configuration mode
You then have access to the AKD parameters that are used when the drive is running.